12/21/2010 5:06 PM | |
Posts: 70 Rating: (0) |
thank u Darius, i think the same that is parameters/configuring problem. here some picture of the configuration in WinCC, i hope that it help you. thanks any way, happy new year to u and yr relatives Attachmentconfiguration.zip (137 Downloads) |
3/12/2012 10:01 AM | |
Posts: 32 Rating: (0) |
I am facing same problem with communication with Wincc via PC adapter if you got solution plz reply. |
3/14/2012 8:02 AM | |
Posts: 32 Rating: (0) |
System parameter set as attached file till not communicate with Wincc. PC which having simatic program communicate and test via PC adapter working ok. PC having Wincc internal tag working fine and checked via PLC simulater found ok. but when communicate plc with winncc not working. AttachmentWincc comm problem via PC adapter.zip (117 Downloads) |
Follow us on