5/11/2016 7:10 PM | |
Joined: 11/13/2008 Last visit: 3/17/2025 Posts: 55 Rating:
|
is possible connect a s7-1200 to op 170 |
5/11/2016 9:26 PM | |
Joined: 3/28/2015 Last visit: 2/15/2025 Posts: 722 Rating:
|
Hello, Kindly have a look at the following topics: 1-TP 170micro, TP 170A, TP 170B, OP 170B (WinCC flexible) Operating Instructions 2-How do you access S7-1200 tags with a panel or RT configured with WinCC flexible 2008 SP2? |
Eng.Mohamed Ibrahim |
|
5/12/2016 4:55 AM | |
Joined: 11/21/2007 Last visit: 3/16/2025 Posts: 2326 Rating:
|
Hello What is the Exact MLFB of the OP170 that you have .. Does it have an Ethernet Interface ? Although , WinCC Flexible allows you to configure Ethernet Connection for OP170B, To the best of my knowledge ( And also as per Technical Details of OP170B ) , and the Manual link in the Post above, OP170B did not have an Ethernet interface. The FAQ posted by Online Tech , though informative, pertains to HMIs with Ethernet Interface. Therefore this FAQ is not relevant for OP170B. Hope this helps. Cheers Navnag |
There is no such thing as the last bug in a program |
|
Follow us on