8/2/2013 2:13 PM | |
Posts: 55 Rating: (0) |
we want to use tcp/ip for communication between s71200 and labview, can u suggest us how we can make it ....... |
8/3/2013 10:29 AM | |
Posts: 3093 Rating: (323)
|
Hello sapnanavre, just have a look at this thread. Ras Sharif wrote he had to insert a special block at labview side. Regards, Kaulquappe |
8/3/2013 4:10 PM | |
Joined: 11/21/2007 Last visit: 8/12/2024 Posts: 2325 Rating: (307) |
Hi sapnanavre There are several ways by which you can connect S7-1200 to labview : a) Profinet - Check out the following links : http://sine.ni.com/nips/cds/view/p/lang/en/nid/210475 b) Modbus TCP/IP Communication /tf/WW/en/Posts/61795#top http://support.automation.siemens.com/WW/view/en/40614428 c) Use OPC Server You can use the OPC linking capability of Labview . http://digital.ni.com/public.nsf/allkb/EA15F53DB6FECCA5862567240064DF09 http://www.ni.com/white-paper/6417/en#toc40 Hope this helps Cheers Navnag |
Last edited by: Navnag at: 8/3/2013 4:53 PMModbus TCP Links added There is no such thing as the last bug in a program |
|
8/14/2013 11:34 AM | |
Posts: 55 Rating: (0) |
hii...........i tried but the problem remained same that's why i am attaching my DB parameters please go through that
Attachmenttcp_hyper.zip (498 Downloads) |
Follow us on