3/15/2023 2:21 PM | |
Joined: 9/12/2019 Last visit: 5/26/2024 Posts: 17 Rating:
|
Hi there, I'm conducting communication tests with a Mypro C-III device, and I'm having trouble reading data from 4 Mycom devices using a CM PtP card. Currently, I'm testing with one device and I should encounter communication errors or other types of errors when testing with the other 3 devices. However, sometimes there are no errors, and the data received from device 1 is received on devices 2, 3, or 4, which doesn't make sense, as they each have a different sending ID. I'm attaching the program and code snippets. Thank you very much for any assistance you can provide. Please let me know if you need further specifications. I do the sending and receiving of data successively, step by step. Best regards, Samuel AttachmentPruebasComMycom_20230315_1519.zip (86 Downloads) |
Follow us on