Industry Online Support
Technical Forum
11/3/2015 2:02 PM | |
Posts: 15 Rating: (0) |
Hello, I have started to work with IEC61850 Communication Block Library for S7-300/S7-400 and I tried to follow the instructions in the manual. But I have a problem. The ERROR output of COM block is high. Also the STATE output must be 12, but it is 13. The following items are used ;
Please look at the attached file(!) for our network structure and the current state of blocks. Please help me ! With best regards. ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 11/5/2015 9:28:21 AMNew subject after splitting |
|
Follow us on