10/8/2020 2:11 PM | |
Joined: 6/30/2014 Last visit: 7/8/2024 Posts: 457 Rating: (87)
|
Dear Kishor, Yes, I know that error message, but: it could have various sources. In the error message box, you see that it could be that you have a local license restricted to a USB-Dongle; The Dongle has to stay connected to the machine where you use the license all the time... if you disconnect it, you will see this error. The Dongle needs an extra driver, is not plug&play. It also could be that you are using a license which comes over the LAN/Local Area Network in your company from a Comos License Server. If the connection gets lost, between the client and the CLS, you will see this error. Or, if the traffic light of the CLS (ComosLicenseServer) is not green anymore, you will get this error message. As we are talking about a tech. issue, it makes no sense to guess which could be the reason for your issue, for me. So, to solve this (in case you have not found yet a solution) would be the best to have a look into it with a ticket, sending your files there. I guess that you do not like to publish your license and logs and so on here, for everybody. Usually, for customers, there is no need to be afraid to open a ticket Here you see the LINK to a good how to document. I hope that this helps you a bit. All the very best, SuperPippo |
Last edited by: Jen_Moderator at: 10/09/2020 07:02:51Optimized link. |
|
Follow us on