1/20/2016 9:54 AM | |
Joined: 5/29/2013 Last visit: 5/2/2024 Posts: 100 Rating: (28) |
5 years later J Let’s make it a little more challenging. I have a DB with 260 variables: bools, bytes, word’s and dword’s all mixed. (no pattern) Can we compare this this easily ? Cause I’m afraid I have to compare them all 1 by 1 now. L
(have to do this in step 7 on a IM151 CPU) ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 1/21/2016 11:08:29 AMNew subject after splitting Regards |
|
1/20/2016 10:20 AM | |
Joined: 6/24/2013 Last visit: 5/2/2024 Posts: 1596 Rating: (410)
|
Hi The compare function attached. I used it many times and it works well. What You supply is - first DB & start address - second DB & start address - length of area to be compared function returns true or false (true when areas are identical) regards Piotr Attachment!FC100_DB_DB_CMP.pdf (808 Downloads) |
This contribution was helpful to3 thankful Users |
Follow us on