6/6/2012 1:48 PM | |
Joined: 3/14/2008 Last visit: 8/3/2024 Posts: 2079 Rating:
|
Hello, I was not able to find the answer in the manuals... I have a program in the cpu,and got the project backupped on disk. How can I check if the project backup is the same as the cpu online program? I saw in the manual that you can compare blocks folder ->Select blocks folder->Options->Compare blocks but I want to check the rest of the project too like CFC charts and also Wincc, the whole project. I saw VXM manager, but unable to select the online project. How do I do that? Thx |
If I could help you, you can use the RATE button. Thank you. |
|
3/11/2013 8:09 AM | |
Joined: 1/3/2006 Last visit: 2/19/2024 Posts: 726 Rating:
|
Hi Yoga shanker, What if there are charts online but not in backup project? |
Follow us on