3/13/2012 3:56 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello, FC10 EQ_STRNG: Compares the content of two STRING-type variables to see if they are "equal". SO, in S1 - input the first variable in format string and in S2 input the second variable in format string. Which functions and IEC standard functions exist in STEP 7 for converting and comparing string variables? How can you copy STRING data types such as e.g. FB/FC parameters and DB variables? Best regards, Hristo MIhalev |
Last edited by: UMENCHO at: 3/13/2012 4:00 PM |
|
3/13/2012 5:45 PM | |
Posts: 288 Rating: (4) |
thanks a lot for your reply mr umencho. can you please give me an example project about using fc10? best regards. |
3/13/2012 7:33 PM | |
Joined: 1/28/2009 Last visit: 4/26/2024 Posts: 6838 Rating: (1359)
|
Please check the attachmnet. AttachmentFC10.zip (802 Downloads) |
3/13/2012 7:40 PM | |
Posts: 288 Rating: (4) |
thank you for your reply mr hdhosseini. please check your email. |
7/5/2017 2:26 PM | |
Joined: 6/19/2017 Last visit: 4/26/2024 Posts: 7966 Rating: (162) |
New question published by Pyeman_999 is split to a separate thread with the subject Boolean latches on and remains true even if the two strings are different?!. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on