7/20/2023 8:45 AM | |
Joined: 5/30/2022 Last visit: 7/17/2024 Posts: 553 Rating: (94) |
Hi Ziemens, The following FAQ shows different ways to review the different functionalities of each HMI model/game: What are the functional differences between the different SIMATIC panels? |
If this information really helps, you could use the Rate function. |
|
7/21/2023 7:54 AM | |
Joined: 8/3/2009 Last visit: 7/17/2024 Posts: 13308 Rating: (1686)
|
Hello Ziemens Do you mean HMI devices like Comfort Panel/ Basic Panels/Advanced RT/Unified Comfort Panel? Or do you mean between HMI types like WinnCC Advanced/Professional/Unified/WinCC V7/8? Which Information do you need exactly? Use the Search function in this forum there are topics from the past that should fit also: (example: LINK) bye Murof |
If this Information really helps, you could use the Rate function |
|
7/21/2023 8:55 AM | |
Joined: 3/2/2007 Last visit: 7/15/2024 Posts: 932 Rating: (5) |
I mean Hmi devices like Comfort Panel / Basic Panels / Advanced . . . |
... thank you ... |
|
7/27/2023 12:45 PM | |
Joined: 8/3/2009 Last visit: 7/17/2024 Posts: 13308 Rating: (1686)
|
Hello Ziemens I do not know any complete list of comparison of all HMI products/devices There is a basic FAQ but it gives you also only links: https://support.industry.siemens.com/cs/ww/en/view/40227286 but WinCC Basic/Comfort/Advanced uses the same technical base. so you can have a look in the systemlimits to check which one fits to your usecases: https://support.industry.siemens.com/cs/ww/en/view/109815056/149280616843 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on