Industry Online Support
Technical Forum
4/7/2014 10:51 PM | |
Posts: 510 Rating:
|
Gavin, I generally I work with the Profinet versions of the panels. The first genration Basic panels come in the Profinet version and the DP version you purchased. The manual, http://support.automation.siemens.com/WW/view/en/31032678 Chapter 5, section 5.1.10describes setting up the the Transfer function on the panel to download theprogram. If you choose serial, it does call out the PPI cable. However, if youselect the DP, you can select the Advanced button to connfigure either DP or MPI. It is a matter of setting theaddress and baud rate. Then you can use the Profibus cable. When Comm ports started disappearing on Laptops I found the docking stations had serial ports that work well with serial communications.(The docking station parallel port also worked well for dongles that used the parallel port.) I use a PG so I can't test it for you. If you have a docking station with a serial portfor the Windows 7 laptop, use the "Setting the PG/PC Interface"and install the PC adapter. Then try to download by selecting the MPI or DP interface and and the PC Adapter. If you don't have a docking station (port replicator), purchasing one may be an economical solution. Let me know if you have success or more questions Regards, billwest |
4/8/2014 8:51 AM | |
Joined: 4/24/2006 Last visit: 7/12/2024 Posts: 8711 Rating:
|
Hello, Perhaps the following links might help: Which connector cables are available for connecting to SIMATIC Panels? Why can you not transfer the HMI configuration to the panel? Best regards, Wizard |
This contribution was helpful to
1 thankful Users |
Follow us on