4/30/2012 1:39 PM | |
Joined: 2/10/2010 Last visit: 3/25/2025 Posts: 77 Rating:
|
Can anybody tell me whether CP-1623 (6GK1162-3AA00) can be used with Windows-7 regards, rajudon
|
4/30/2012 1:49 PM | |
Posts: 133 Rating:
|
Hi rajudon Yes the CP1623 is compatible with Windows XP, Windows 7 as well as Windows 2008 Server. I have used it and it works. |
4/30/2012 4:26 PM | |
Joined: 2/10/2010 Last visit: 3/25/2025 Posts: 77 Rating:
|
Thank you very much to everybody regards, rajudon |
4/30/2012 5:18 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating:
|
Hello, Further Important questions thatare related toyour start question: What Simatic Net CD version do you require to run Windows 7? And do you run Win7 in 32 bit or in 64 bit version? The answers to these questiosnchange the minimum software requirement. There are some FAQ giving the response to that kind of questions. Which SIMATIC NET CD is released with which Microsoft Windows operating system http://support.automation.siemens.com/WW/view/en/25246170 Compatibility Tool http://support.automation.siemens.com/WW/view/en/56699648 |
Best regards |
|
4/30/2012 9:19 PM | |
Joined: 4/19/2008 Last visit: 11/21/2024 Posts: 1525 Rating:
|
Hello A Small Addition to Above ... In which PCI slots can you operate the different Industrial Ethernet and PROFIBUS PC CPs? Which SIMATIC NET Industrial Ethernet PC CP is compatible with which Microsoft Windows operating system? |
Ammy |
|
9/8/2014 11:41 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4766 Rating:
|
New question published by Shreyasis split to a separate thread with the subject how to procure the driver for windows7 as the PC doesnt initialise the CP 1623 ethernet ports? Best Regards Min_Moderator |
Follow us on