5/28/2021 6:09 AM | |
Posts: 1 Rating:
|
i have windows 10 laptop but v14 sp1 not comparable for this |
12/15/2022 2:36 PM | |||
Joined: 7/7/2010 Last visit: 9/6/2024 Posts: 15157 Rating:
|
Portal prior to V13 SP2 Update 4 do not have the required security protocol support (TLS 1.2) to connect directly to Siemens Update Servers. FYI, V13 SP2 Update 4 must be downloaded from this support site directly - or order an install DVD package, if they are still available. As far as I know, there is no V13 SP2 update that works with the current security protocols (TLS1.2). Hope that is useful. => Meaning, you need to manually download and install the entire package "V13 SP2 Update 4" as a complete install package. Not "update 4" to V13 SP2. Very different. The updater is not going to be your friend on V13 unless you have a local Siemens Update Server at your company configured to work with V13 (not likely).
|
||
science guy |
|||
12/15/2022 7:24 PM | |||
Joined: 3/1/2018 Last visit: 7/30/2023 Posts: 8 Rating:
|
Portal prior to V13 SP2 Update 4 do not have the required security protocol support (TLS 1.2) to connect directly to Siemens Update Servers. FYI, V13 SP2 Update 4 must be downloaded from this support site directly - or order an install DVD package, if they are still available. As far as I know, there is no V13 SP2 update that works with the current security protocols (TLS1.2). Hope that is useful. => Meaning, you need to manually download and install the entire package "V13 SP2 Update 4" as a complete install package. Not "update 4" to V13 SP2. Very different. The updater is not going to be your friend on V13 unless you have a local Siemens Update Server at your company configured to work with V13 (not likely).
Can you give me an advice what to do if I want to upgrade to V14 or higher if possible without breaking the bank. This is my private PLC. Thanks. |
||
Follow us on