10/11/2019 2:06 PM | |
Joined: 2/24/2015 Last visit: 1/25/2023 Posts: 306 Rating: (76) |
Do you call it in OB3x? |
10/14/2019 8:46 AM | |
Joined: 5/3/2017 Last visit: 5/21/2024 Posts: 673 Rating: (217) |
Hello AutoGen_4691648, normally the inputs for the controlling from WinCC (i. e. AutModOp) will reset automatically, but if you interconnect the input this won't work (the signal from the interconnection is used). So the only way I know is to adapt the faceplate. In the manual PCS 7 APL Style Guide at section "Binary value operation APL_OP_BUTTON" you can find the information how to reset a digtial input from WinCC. With regards |
Follow us on