1/29/2019 7:23 PM | |
Joined: 3/15/2018 Last visit: 7/5/2024 Posts: 13 Rating:
|
Hello there, I need help about the comunication via MODBUS TCP IP with S71500 and Serie Q .(Q03UDVCPU) Thanks |
1/29/2019 7:29 PM | |
Joined: 9/27/2006 Last visit: 4/19/2025 Posts: 12346 Rating:
|
Hello Fabio; Look at the following discussion: communication between S7 1500 CPU and Mitsubishi PLC Study the communication capabilities of your Mitsubishi CPU, then see if one of the mentionned protocols will match with the S7-1500 networks. Hope this helps, Daniel Chartier |
This contribution was helpful to
1 thankful Users |
1/29/2019 7:34 PM | |
Posts: 2826 Rating:
|
Plus:
Both sides map Modbus addresses to internal-to-the-PLC addresses. The communication is only concerned about linking the Modbus addresses. Look at the provided materials and see what you can extract from it. Good luck. |
1/30/2019 6:01 PM | |
Joined: 3/15/2018 Last visit: 7/5/2024 Posts: 13 Rating:
|
Thank you very much! |
This contribution was helpful to
1 thankful Users |
Follow us on