4/14/2010 11:20 AM | |
Joined: 9/19/2009 Last visit: 3/15/2025 Posts: 459 Rating:
|
Comunication with CP5511. Hello everybody. I know that there is others FAQ about the CP5511 but don´t help me. I followed the next: How do Diagnostics and Remedy work in STEP 7 when an online connection with the CP5511 is not possible? This was my mistake:0x0316 Hardware resource already occupied: So, I followed this link: How can SIMATIC NET software communicate correctly with the CP 5511 in Windows 2000/XP The problem is that this link tell me, I need memory resources "D0000-DFFFF" , but in my computer I have Attachment: When I go to PC/PG interface, and diagnostic CP5511, I press the test and the computer not Responding.I need shut down the computer every time. I don´t know where is the problem, If anyone can help me! Thanks advanced Regards JM AttachmentMicrosoft Word - CP5511.pdf (95 Downloads) |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
4/24/2010 4:25 PM | |
Joined: 9/19/2009 Last visit: 3/15/2025 Posts: 459 Rating:
|
Thank you for your Reply I think that the best solution is change it. I lost a lot of time. I try format the computer but the problem is the same. I will try with old computer. Thank you very much Regards JM |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
This contribution was helpful to
1 thankful Users |
Follow us on