7/5/2009 2:35 PM | |
Posts: 13 Rating: (0) |
HI all is there way to concatenate two integers. eg. int1 =4A int2=50 total= 4A50 Is there a standard FB that i could use. Mags |
7/5/2009 8:54 PM | |
Joined: 4/5/2006 Last visit: 10/10/2024 Posts: 917 Rating: (63) |
Hi mags, IBN-Servicesaid you right, if you want concatenate you have to shift the MSB on the left.. I just got a lil confusion about what you asking: in the title of tread speak about BYTE (8 bits), in the question speak about INT (16 bits), operation doesn't change ... just remeber to shift MSB by 8 or 16 (or multiply x 256 or 65536)...format is important too for right result Regards |
7/6/2009 5:53 AM | |
Posts: 2661 Rating: (279)
|
Hi mags, What you need is possible from the method I suggested. Give it a try and let me know. Regards |
Follow us on