10/12/2022 4:39 AM | |
Joined: 3/14/2008 Last visit: 8/3/2024 Posts: 2079 Rating:
|
Hi, There could be several issues like the user names are not the same between PC stations or the passwords differ from each other. The user is not part of Simatic HMI group. Under the Siemens installed directory you can find a tool to set rights to specific folders: It's called Simatic Rights and configures settings that are needed. Have you executed this Is the installed software the same? |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
1 thankful Users |
Follow us on