8/19/2023 4:14 PM | |
Joined: 12/18/2014 Last visit: 1/17/2025 Posts: 34503 Rating: (4306)
|
I think the sensor outputs AC, not DC. |
This contribution was helpful to1 thankful Users |
8/19/2023 5:18 PM | |
Joined: 6/11/2019 Last visit: 1/16/2025 Posts: 2400 Rating: (112) |
Hello sionshine, the sensor cannot be used for the Logo without an additional converter or converter circuit. He's more like an Adoino, RPI or ESP. Better to buy directly what fits the logo according to the norm. An example of this would be the AT-100 B10, or AT-B420L from the AT-B series from LEM. Greetings Ella_68 (translated with Google) |
This contribution was helpful to1 thankful Users |
8/20/2023 7:51 AM | |
Joined: 6/11/2019 Last visit: 1/16/2025 Posts: 2400 Rating: (112) |
Why ? , It´s a Logo-Forum ! |
Follow us on