1/28/2013 12:26 PM | |
Joined: 8/31/2010 Last visit: 9/24/2024 Posts: 1521 Rating: (227) |
Hello spandan, It's better to raise a Support Request in parallel to this discussion - Support Request As they may be able to provide a solution quickly. Two of us here when we can click the "Start Device Tool", it must be specific to the installed PG/PC. |
Like it? Rate it! |
|
1/28/2013 1:12 PM | |
Posts: 17 Rating: (1) |
I have already made a service request to Siemens. But can u explain here in brief the steps to proceed for the configuration of the IO-Link Master. It might be that I am missing something here. |
1/31/2013 6:24 AM | |
Joined: 8/31/2010 Last visit: 9/24/2024 Posts: 1521 Rating: (227) |
Hello spandan, There is a new Function Manual on SIMATIC IO-Link system is released. See if this helps you. |
Like it? Rate it! |
|
Follow us on