11/17/2017 1:36 AM | |
Posts: 2 Rating: (0) |
Hi all. I have a machine here with a 1200 CPU and an S120 drive with a CU-320-2 PN. The machine was built in another country and imported. Machine runs ok most of the time, however it will randomly issue a "Main Controller Fault" on the HMI and fail to run until machine power is cycled. I initiated a connection with TIA V14, which shows me a demand maintenance error on the profibus of the drive stating "No diagnostics data available because the current online configuration data differs from the offline configuration data". My question is - I can't seem to find the correct TIA support package for the S120 so i can upload the configuration from the drive and update the project file. So far i have tried DriveLib V50 (https://support.industry.siemens.com/cs/ww/en/view/109475044) with no luck. I have downloaded Starter V4.5 and managed to go online with the drive ok. Is there a way i can update the TIA project with the drive parameters uploaded from starter? Any help would be greatly appreciated! Thanks. Ben |
Last edited by: Bwilliams at: 11/17/2017 1:44:06 AMLast edited by: Jen_Moderator at: 11/17/2017 10:22:45 AMInserted right link. |
|
3/5/2019 8:01 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (173) |
New question published by SdSady is split to a separate thread with the subject Communicate S120 drive with CU320-2PN. Best regards |
Follow us on