8/2/2011 10:37 AM | |
Posts: 1547 Rating: (129)
|
Hi Impsi, I'm not sure, but I would advise you to install the SP5 first: http://support.automation.siemens.com/WW/view/de/36184684 If not working with this you should contact the Siemens hotline; they can also give you the latest hotfix (8) for V.5.4.5. Regards, Rated X |
8/3/2011 12:41 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (308) |
Hello, Look at this link (download firmware for IM151) http://support.automation.siemens.com/WW/view/en/35934244 You will see the following sentence for V7.0 Note on STEP7: Replacement, compatibility and configuration A configuration change is only necessary if the new function of the FW V7.0 are to be used. In this case you require Step7 V5.5 for the configuration. |
Last edited by: jklm at: 8/3/2011 4:11 PMLast edited by: jklm at: 8/3/2011 3:09 PMBest regards |
|
Follow us on