5/5/2014 8:40 AM | |
Joined: 12/12/2011 Last visit: 12/30/2020 Posts: 821 Rating: (40)
|
Hi banconi, yes,electronigsignature would be a possibility. Here is an application http://support.automation.siemens.com/WW/view/en/67688514 Best Regards, Healthcheck |
Last edited by: GrasserF at: 5/5/2014 9:07 AMedit Link de/en Last edited by: Healthcheck at: 5/5/2014 8:42 AMGrundkurs/Systemkurs WinCC V7: |
|
This contribution was helpful to3 thankful Users |
5/15/2014 6:56 PM | |
Joined: 10/20/2009 Last visit: 4/3/2017 Posts: 215 Rating: (12) |
Hi banconi, Please go to below link: https://www.automation.siemens.com/tf/WW/en/Posts/14349 Here they have given c script to make a message box. |
Regards, |
|
5/16/2014 3:46 PM | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Joined: 10/20/2009 Last visit: 4/3/2017 Posts: 215 Rating: (12) |
Hi, You can use following commands to make confirmation box using VB script: DescriptionDisplays a message in a dialog box, waits for the user to click a button, and returns a value indicating which button the user clicked.SyntaxMsgBox(prompt[, buttons][, title][, helpfile, context]) The MsgBox function syntax has these arguments:
|
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Regards, |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
This contribution was helpful to2 thankful Users |
5/16/2014 5:04 PM | |
Joined: 10/3/2010 Last visit: 5/17/2024 Posts: 1552 Rating: (188) |
Siemens solution from FAQ: http://support.automation.siemens.com/WW/view/en/26729052 There are also several others ways, for example creating your own pdl with buttons Yes and Cancel. this pdl you can put in an invisible picture window on your screen or startscreen. Clicking the I/O-field, you can make your picture window visible. Cancel just closes the picture window, Yes executes your code. VBS-msgbox is not recommended as it can pause other running script, which can cause serious problems? If you want, you can also play with Operator-Control Enable. Set "Operator-Control Enable" of the "dangerous" I/O-fields by default to "No", make an internal binary tag like "OperationEnabled" which you can manipulate on your screens by having an extra button "Enable/Disable setpoints". This button toggles the internal tag and link this tag to the "Operator-Control Enable-property of your I/O-fields. Other option is using different users. Choices enough. |
B r g d s , |
|
5/16/2014 6:33 PM | |
Joined: 11/26/2011 Last visit: 6/29/2023 Posts: 508 Rating: (22) |
With user rights also you can do ..... |
5/19/2014 5:04 PM | |
Joined: 7/19/2011 Last visit: 4/27/2024 Posts: 262 Rating: (5) |
R J method is the best and user friendly . Thanks for the post |
JAVED AKHTAR |
|