9/10/2018 4:44 PM | |
Joined: 12/18/2014 Last visit: 3/25/2025 Posts: 34937 Rating:
|
The relay contacts of both the base module and the expansion module are potential-free on the terminals. |
9/11/2018 8:33 AM | |
Joined: 12/18/2014 Last visit: 3/25/2025 Posts: 34937 Rating:
|
Here's an example of the wiring. The 12 VDC can be switched via each relay contact, also via the relays of the base module. AttachmentUntitled.pdf (236 Downloads) |
9/11/2018 8:50 AM | |
Posts: 10 Rating:
|
Thank you, I got it now! 5 stars for you. |
This contribution was helpful to
1 thankful Users |
9/11/2018 8:53 AM | |
Joined: 12/18/2014 Last visit: 3/25/2025 Posts: 34937 Rating:
|
Hello mmatt111, you're welcome... |
Follow us on