3/10/2019 6:16 AM | |
Posts: 9 Rating:
|
Dear Sir, Hi Thanks for sharing your project with us it was very helpful. I have a similar project in which i have to connect 4 (up to 6) Load cells to a S7-1200 PLC through a Modbus transducer (made for load cell). In this project i have to read some values from the transducers (like weight...) and write some values (for calibration of the weighing system). Can i use your procedure? It's for a cement batching plant. It has cement weight, water weight, additive weight (maybe 2), and aggregate weight. I need to weight these and open or close gates or valves or run a conveyor belt. how fast can i weight this 4? can it be somehow seamless and feels like they are at the same time? I know how Modbus-485 works. let's say it's about 2000kg aggregate, 400kg water, 500kg cement and 50kg additive. thanks for your help ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/11/2019 9:14:38 AMNew subject after splitting |
|
3/18/2019 7:46 AM | |
Joined: 6/19/2017 Last visit: 12/4/2023 Posts: 7588 Rating:
|
Closed cause question posted twice. The second thread with the subject Questions regarding cement batching plant is published within the conference Process Instrumentation / Analytics / Weighing Systems SIWAREX. Best regards Jen_Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on