4/23/2019 7:00 PM | |
Posts: 10 Rating: (0) |
Hello everyone, in my project i need to connect a PC Station to an S7-1200 using OPC-ua , for that I´m using this application description: https://support.industry.siemens.com/cs/ww/en/view/39960679 For a long time I'm stuck in the stage of Compiling and Downloading the PC Station Configuration,when I try to download the PC Station, we detect just the plc which is not the case in the application description (please see picture_1 below). I believe the problem comes from the step just before that is to insert the OPC server and the IE general in the Station Configuration Editor. when I add the IE general I can not change the properties (ip and mac addresses) for that be in accordance with the hardware configuration and then connection is established. thank you for helping to solve this problem. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 4/24/2019 11:37:34 AMNew subject after splitting Last edited by: Jen_Moderator at: 4/24/2019 11:39:43 AMOptimized link. |
|