7/3/2018 3:55 PM | |
Posts: 80 Rating: (2) |
Is it possible to connect a Raspberry camera module v2 to the IOT2040? Is there any way or connector to do it? |
7/4/2018 1:59 PM | |
Joined: 4/28/2015 Last visit: 5/15/2024 Posts: 3345 Rating: (377)
|
Hi, for me it is not clear what the costumer wants to do with camera picture on the IOT, beacause there is no display / desktop like on the raspberry pi. Or is he displaying the picture on a website running on the IOT? Even if there is a connector, the CSI protocol has to be adapted. I am not sure if this is possible to emulate CSI with the GPIOs. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
7/4/2018 3:15 PM | |
Posts: 80 Rating: (2) |
He wants to take the pictures and send them via FTP to the IT department. The IT department then use the pictures in different dashboards. |