Industry Online Support
Technical Forum
12/4/2014 8:43 AM | |
Posts: 1 Rating: (0) |
Can you only configure a HMI in Step 7 if you have WinCC flexible. I have Step 7 as well as WinCC Runtime. Updated WinCC but still can't add a HMI station into the project. Would like to connect a S7-317 and a KTP600 HMI in step 7 and then figure out a way to setup the HMI screens.
----------- new subject after splitting from Integration of HMI siemens station into Simatic manager |
Last edited by: CS Moderator at: 12/4/2014 11:24 AMsplitting |
|
12/4/2014 11:37 AM | |
Joined: 4/24/2006 Last visit: 5/1/2024 Posts: 8629 Rating: (1147)
|
Hello, Perhaps the following link might help: Combined configuration with WinCC (TIA Portal) and STEP 7 V5.x Best regards, Wizard |
Follow us on