10/22/2024 7:53 AM | |
Joined: 2/26/2018 Last visit: 3/20/2025 Posts: 4 Rating:
|
Hi, I've got the logging in using the script working, howerever i'm stuck with a problem. Whenever I loging using the script my language changes from dutch (default) to english (second). is there a way to connect a user with a specific language to prevent this switching? In the trace viewer I get the following entry: trace: User Change for client DESKTOP-7O46EBE succeeded. User: Operator | Language: 1033 Thanks in advance! - Nick ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 10/22/2024 08:09:48New subject after splitting |
|
10/22/2024 11:37 AM | |
Joined: 2/26/2018 Last visit: 3/20/2025 Posts: 4 Rating:
|
Yeah, I can find a workaround maybe, but why does it change the language in the first place? |
10/22/2024 11:52 AM | |
Joined: 11/28/2023 Last visit: 2/26/2025 Posts: 21 Rating:
|
Hi NickK96, not sure if the language switch is intended. Anyway there is an official workaround for that: See 4.2 in Click me Like mentioned earlier just add a script triggered by @UserName and activate the language you want. Best regards, |
This contribution was helpful to
2 thankful Users |
Follow us on