12/31/2013 11:21 AM | |
Posts: 8 Rating: (0) |
Dear sir i need your help to know how could connect and make program for encoder with 2 puls 4 wires to seimens PLS S7-300 |
1/2/2014 5:03 PM | |
Joined: 4/22/2010 Last visit: 11/18/2024 Posts: 5697 Rating: (715)
|
Hello, Looks like you have a motor like in attached document. At page 9 you can read about the Encoder. A2 phase encoder is a special option. The encoder is a 5 Volt one if you want to connect it to a PLC you need to convert the 5 V signal to 24V pulses (optocoupler i.e.) or a 5V counter card. Regards, Marcjan AttachmentDCmotors601-0241.pdf (551 Downloads) |
Problem solved? |
|
1/2/2014 5:21 PM | |
Joined: 3/21/2006 Last visit: 11/1/2024 Posts: 10229 Rating: (1181) |
Search for high speed inputs either in CPU31x or in FM350-1 or FM350-2 ... as suggested byMarcjan. |
Follow us on