8/20/2012 11:57 AM | |
Posts: 1547 Rating: (129)
|
Hello hieutran8969Look at this link. Configuring an ET 200S as PROFINET IO device. That is a full example for the configuring. |
This contribution was helpful to2 thankful Users |
8/20/2012 12:02 PM | |
Joined: 4/24/2006 Last visit: 5/8/2024 Posts: 8638 Rating: (1151) |
Hello, Here is manual of newer type: SIMATIC ET200S distributed I/O Interface module IM151-3 PN High Feature (6ES7151-3BA23-0AB0) perhaps it might help. You should give IM151-3 the right IP address and a Device name. (they should match the Hardware configuration) Best regards, Wizard |
8/21/2012 9:05 AM | |
Joined: 4/24/2006 Last visit: 5/8/2024 Posts: 8638 Rating: (1151) |
Hello, Did you connect the Terminator (small 5mm) at the end of ET200S rack? Best regards, Wizard |
8/27/2012 2:54 PM | |
Posts: 1547 Rating: (129)
|
Hello hieutran8969Is your ET200S in the window “Assign device name” available? |
Follow us on