4/29/2015 9:01 AM | |
Joined: 4/16/2015 Last visit: 12/2/2023 Posts: 2 Rating:
|
Warm greetings. can anyone help me to figure this out: I have Wincc flexibale SP1 and PPI-RS485 multi master cable (6es7 901-3cb30-0xa0). and recently I've been trying to download projects on (TP 177B, TP 177A, MP 277A) but only the 177A connected via the cable (others can connect via ethernet). *I have noticed that the 177A OS is FREE and differs from the others* and I think this has something to do with the issue. Sorry for asking this in a comment but the forum won't allow me to post due to internal error
---------------------------------------------------------------------------------------------------- |
Last edited by: Hasan_MZ at: 4/29/2015 9:02:58 AMLast edited by: Hasan_MZ at: 4/29/2015 9:03:19 AMLast edited by: Hasan_MZ at: 4/29/2015 9:03:34 AMLast edited by: Min_Moderator at: 4/29/2015 4:41:47 PMNew subject after splitting |
|
Follow us on