5/10/2017 4:31 PM | |
Posts: 2 Rating: (0) |
Hello i have a S7-200 224-Cpu and i have only a profibus cable. Can i connect my pc with plc with profibus(male/male) cable with a male/female adaptor?Or i have to buy a ppi cable? Thanks. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 5/11/2017 1:45:39 PMNew subject after splitting |
|
5/10/2017 7:21 PM | |
Joined: 3/28/2015 Last visit: 5/10/2024 Posts: 721 Rating: (213) |
Hello, Kindly have a look at the following topics: PROFIBUS PC Adapter USB A2 Operating Instructions The PPI bus profile can be used via the "Universal" PROFIBUS bus profile |
Eng.Mohamed Ibrahim |
|
This contribution was helpful to2 thankful Users |
Follow us on