7/12/2016 10:34 PM | |
Posts: 1 Rating: (0) |
Hello guys, I need to connect a PLC Panasonic to WinCC by Modbus RTU, is it possible to do directly? I Tried to read coils, inputs. Force coils, but with no sucess. I think the adress is correctly, could you help me? Attached are images of the WinCC ------------------------------------------------------------------------------------------ AttachmentPictures.zip (174 Downloads) |
Last edited by: Min_Moderator at: 7/13/2016 12:19:04 PMNew subject after splitting Last edited by: Min_Moderator at: 7/13/2016 12:20:49 PMAdd attachment |
|
This contribution was helpful to1 thankful Users |
Follow us on