4/18/2012 9:30 AM | |
Posts: 1 Rating:
|
me to please if you achive information about it forward information for me.
|
4/18/2012 9:51 AM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating:
|
Hello, See attached pictures for more details Regards, Marcjan Attachmentcp-connection.pdf (148 Downloads) |
Problem solved? |
|
4/25/2012 11:53 AM | |
Posts: 24 Rating:
|
Thanks for these detail, but I have always a problem to connectmy logo! 0ba7 with my s7-300. Someone can identify the problem ? Thank you, AttachmentS7_Logo.zip (89 Downloads) |
4/25/2012 4:53 PM | |
Posts: 1547 Rating:
|
Hello, the LOGO can be connected via S7 connection. For this you need a plc which supports the PUT GET Function. Add a Ethernet CP to your plc. Create Ethernet Network and add an S7 connection. The connection MUST be established by S7 PLC. for Rack and Slot put 0. Here you will find a sample with S71200 PLC instead S7 300, but the way on LOGO is the same. Application examples for LOGO! direct download : http://www.automation.siemens.com/salesmaterial-as/software/applications/logo/s7-1200_communication.zip To follow this sample you have to choose a connection resource also the 20 in Net Pro. |
Follow us on