4/18/2018 11:01 PM | |
Joined: 6/5/2014 Last visit: 4/25/2021 Posts: 109 Rating: (1) |
Dear all, Any Update. Best Regards, |
4/19/2018 1:22 AM | |
Joined: 9/27/2006 Last visit: 5/22/2024 Posts: 12257 Rating: (2668) |
Hello Mahmoud; Since there are no drivers for SNP in WinCC v14, you will need to use an OPC server. In the doculent below you can e¸determine the type of OPC server, based on the pltform you are using, Runtime SCADA or panels. https://support.industry.siemens.com/cs/ww/en/view/109747181 You can then look for an adequate OPC Server form Matrikon, Top Server, Kepware... Hope this helps, |
Last edited by: dchartier at: 4/19/2018 1:23:22 AM |
|
This contribution was helpful to2 thankful Users |
4/19/2018 12:18 PM | |
Joined: 3/16/2014 Last visit: 10/14/2021 Posts: 120 Rating: (66) |
In TIA 15.0 you can also connect to Fanuc I think using the OptionPack: SINUMERIK - Create MyHMI. I do not know if this kind of connection is what you are looking forward. https://support.industry.siemens.com/cs/ww/en/view/109752377/105703147019 |
Last edited by: Jen_Moderator at: 4/19/2018 2:25:48 PMOptimized link. |
|
This contribution was helpful to1 thankful Users |
3/7/2023 9:03 AM | |
Joined: 12/23/2020 Last visit: 3/7/2023 Posts: 24 Rating: (1) |
hi how it can be done? thanks |
Follow us on