11/11/2019 2:30 PM | |
Joined: 4/29/2019 Last visit: 12/3/2023 Posts: 11 Rating:
|
Dear All I have similar problem, and it looks this issue is not solved yet. Can you please help? I have to connect two TP1200 comfort panel to a CPU314. This CPU has only MPI connection. And only one of it. CPU program is written in simatic manager V5.5 and the HMI is not integrated in it nor in HW config. Currently the equippment is running with one HMI and we have to duplicate it. What I did till now: Backup from the old panel and restore the hmi project to the new HMI. Modified its address to 3. Modified the number of OP communication in the CPU HW config from 1 to 2 and downloaded. With this configuration it does not work. The new hmi with the address 3 does not connect. I have tried the same address for both HMI, so address 1. In this case either the one or the other is conncecting. It depends on which one I plug in later. CPU address is 2. The current addresses: CPU: 2 HMI_1: 1 HMI_2: 3 there is no other communication. What else could I try? Thank you for your help! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/12/2019 07:48:44New subject after splitting |
|
Follow us on