1/27/2012 2:30 PM | |
Joined: 10/9/2007 Last visit: 9/26/2024 Posts: 1250 Rating: (115)
|
Hi If the device is new, you should configure it directly in Digsi, then download to the device. The "default configuration" from a new project from Digsi is the same project you have on the device. So you don't need plug&play. Plug&Play has to be done only if you don't have the backup. If the device is using protocols like IEC61850 you can do plug & play, but you cannot change the configuration, only adjust settings such as protection parameters. Some other information from the device cannot be retrieved using Plug&Play, like long texts and commentaries from CFC. So I recommend keeping and using the Backup, instead relying on Plug&Play. In chapter 7.2 you find the description about Plug&play http://siemens.siprotec.de/download_neu/devices/1_General/System_Manual/SYSTEM_MANUAL_B4_SIPROTEC4_DIGSI4_EN.pdf This is manual shows the basic steps in Digsi http://siemens.siprotec.de/download_neu/software/DIGSI_4/Manual/DIGSI_STARTUP_A5_EN.pdf Mike |
Last edited by: Mike J at: 1/27/2012 2:32 PMEnergy Automation products: Sicam, Siprotec, Digsi |
|
1/29/2012 6:47 AM | |
Posts: 5 Rating: (0) |
Hi Mike, I have tried doing what you have indicated about 'Plug & PLay' but still i have not been able to communicate with the relay. I am using a cross cable as well (U1110 from Moxa) Some information on settings and systems i am using: OS : Windows 7 Enterprise DIGSI : 4.83 SIPROTECH : 7SJ622 MLFB : 7SJ6225-5EB003FEO Firmware : FIRMWARE V04.64.01 Interface cable: U1110 specs above in hyperlink I am trying to connect via Direct connection using PC interface COM1 and frame '8E1' setting. I have tried to connect at 9600bps using flow control 'None' and also at 38400bps(which is indicated in the relay. Hope this info helps you to troubleshoot my problem. Regards Vinay |
12/26/2013 11:47 AM | |
Posts: 5 Rating: (0) |
Good Morning, Keep on trying... I'm sending the screens with the communication port (interface) configurations. My language is portuguese, so if it's not clear, please ask for clarifying. Thank you, Ijano.
AttachmentDigsi - Configuração Interface Rele.zip (692 Downloads) |
Follow us on