10/31/2006 11:30 AM | |
Posts: 78 Rating: (3) |
hi J_Bell, thanx for ur reply, I think that it has consistent data of a byte, and I'm sure, I need more than 4 bytes and I connected the slave to the master system. would u plz do me favour, I attach the GSD file , plz check this out and tell me more about what I have to do after installing it and connecting to the master system, thanx a lot. AttachmentDIRI0948.zip (1108 Downloads) |
11/7/2006 10:39 AM | |
Posts: 5822 Rating: (411) |
Well, this is relative simple, CFC has problems handlich ANY Pointers. Here you need an ANY Pointer. The ANY Pointer directs the data to the destination field. in your case you need for the Record something that would look inSTD like: p#db1.dbx0.0 byte 34 for your Inputs and p#db2.dbx0.0 byte 29 foryour outputs. How this is done in CFC, I have no clue. This you should ask a CFC specialist. Maybe this helps: "Connecting" the ARRAY type ANY pointer in CFC Best regards |
Follow us on