11/7/2011 12:40 PM | |
Joined: 9/23/2005 Last visit: 9/10/2025 Posts: 4416 Rating:
|
Hi, what is the PLC that you use? |
Denilson Pegaia |
|
11/24/2011 11:40 AM | |
Posts: 44 Rating:
|
Hi sory for the late reply, I am back on this project now, The plc is 1200 1212C The data sheet for the encoders is attached, the model sepcification is 5000.7154.4096 which means Push Pull output with inverted signal ( power supply 10-30v dc) M12 8 pin connector Pulse rate 4096 My undetstanding of these encoders is low and the help from the UK supplier is poor. Simple questions (perhaps not simple answers ![]() From this encoder how many cables would I connect into the plc , 1 or 2 ? How would I read/count the pulses from the encoder within the PLCto determine an dimension. Attachment5000-5020_en.pdf (1255 Downloads) |
Follow us on