5/26/2008 2:59 PM | |
Posts: 5822 Rating:
|
Dear alfie, I would say... try it! I think you will not get the supply for the TTY Loop easier than that. Best regards J_Bell |
5/27/2008 10:56 AM | |
Posts: 5822 Rating:
|
Dear Alfie, do it. If the device you have is worth it, it has to work. The pin 11 and 13 are the Supply for the +20mA TTY Loop. Best regards J_Bell |
5/28/2008 9:40 AM | |
Posts: 5822 Rating:
|
Hello alfie, this is strange, we tested this with a SIMAITC PC/AS511 Cable. Do you use a cable by another vendor? Best regards J_Bell |
5/31/2008 6:43 AM | |
Posts: 2 Rating:
|
Hi, Alfie, The pin 14 you have used is not suitable to feed power into current loop, because it is named on the page 3-25 of the CP143TF manual (se attachment in private post) as "Master scan", therefore, this is simply signal output of logic IC. You can not use this IC output as source for 20 mA loop, due to the fact that this signal has no enough power and potentially has not stable voltage level. AttachmentRS232TTY4.pdf (402 Downloads) |
Follow us on