9/11/2008 10:38 AM | |
Posts: 19 Rating: (0) |
Hi, I want to connect RF660R with CPU 315-2 PN/DP via TCP/IP protocol. How can I do this? Could you please tell me how to do? Regards, Emin |
9/11/2008 1:50 PM | |
Joined: 9/27/2006 Last visit: 5/2/2024 Posts: 12257 Rating: (2666) |
Hello bodemin; I found the following Application example from the Siemens support website: "Connecting a SIMATIC RF660R read / write device to SIMATIC S7 315-2PN/DP" Think it could help? http://support.automation.siemens.com/WW/view/en/23626344 You can download code for an example program from this link as well. . Hope this helps, Daniel Chartier |
9/11/2008 2:30 PM | |
Posts: 19 Rating: (0) |
Thanks for your assist. I have found this program too. But I couldn't use it. It is some complicated. And I got some errors. For example, I cannot switch the PLC to RUN mode. |
Follow us on