3/21/2010 2:07 PM | |
Posts: 4 Rating: (0) |
Hi, which CPU 200 you use? Which adapter u have to connect CPU And PC(or panel)? And which panel you want to use? |
3/21/2010 5:16 PM | |
Posts: 691 Rating: (37) |
Better check the communication defined for the WinCC Flexible Runtime and match the same in the Set PG/PC Interface Setting |
3/22/2010 5:03 AM | |
Posts: 13 Rating: (0) |
yes.. i've checked access path S7 online, i set same in PG/PC interface.. is it possible to communicate with PC/PPI cable..? |
3/22/2010 5:47 AM | |
Joined: 3/21/2006 Last visit: 11/1/2024 Posts: 10229 Rating: (1181) |
Hello Naveen, Yews it's possible to use PPI. Look at What should you watch out for when setting up a connection between S7-200 and SIMATIC Panels or WinCC flexible PC Runtime and what are the options? and about problem with missing USB interface in PG/PC options look at Why does the menu option "USB" disappear from the list box in "Set PG/PC interface" as soon as WinCC flexible 2005 is installed if "PC/PPI Cable (PPI)" is enabled on the "Local Connection" tab? Hope this will help. Best regards, Hristo Mihalev |
3/24/2010 3:42 PM | |
Posts: 4 Rating: (0) |
Did you try to set PG/PC via Step7 if you have instaled? |
Follow us on