9/21/2019 2:15 PM | |
Posts: 20 Rating: (0) |
Hi, Please can anyone send connection & configuration details of KP300 HMI with S7 1200 through intermediate switch. Thanks ------------------------------------------------------------------------------------------ |
Last edited by: CS Moderator at: 09/21/2019 23:52:07New subject after splitting |
|
9/21/2019 2:28 PM | |
Joined: 9/27/2006 Last visit: 4/26/2024 Posts: 12257 Rating: (2665) |
Hello nraza; See if the hints provided in this discussion can help you out. On e of the HMI connected to the S7-1200 CPU in this thread is a KP300. How connect two hmi to plc cpu s7 1200 Note that if the switch is present in the physical network, it is not configured as part of the Profinet connection between the PLC and the HMI stations. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 09/21/2019 14:31:39 |
|
Follow us on