12/12/2011 7:18 AM | |
Posts: 88 Rating: (1) |
Dear Umencho, I've read your guideline in manual, but I'm confused about the two possible connections. I've attached a picture in which the two possible connections are shown. Any reference to any document or any guide is appreciated in advance. Best Regards, |
Last edited by: O_Moderator at: 12/13/2011 7:52 AMnew subject after splitting from /tf/WW/en/Posts/59410#top |
|
12/12/2011 7:33 AM | |
Joined: 3/21/2006 Last visit: 10/7/2024 Posts: 10229 Rating: (1181) |
Use above mentioned FAQ and look at attachment. Best regards, Hristo Mihalev |
12/22/2011 11:46 AM | |
Posts: 27 Rating: (1) |
Hi! I think the attached picture looks ok. Each redundancy modul get 24V and 20A max. |
9/16/2014 9:00 AM | |
Joined: 8/18/2014 Last visit: 8/29/2024 Posts: 2 Rating: (0) |
Dear Late Thanks for your advise. Have a look to the attached PDF file page 2 ... this is typical to what you said.
AttachmentSITOP_modular_Redundanz_SB_en.pdf (839 Downloads) |
Thanks, |
|
9/2/2021 8:47 AM | |
Joined: 1/28/2021 Last visit: 4/14/2023 Posts: 2 Rating: (0) |
i need wiring diagram and working of it. request you to please help. |
Follow us on