9/2/2021 11:23 PM | |
Posts: 257 Rating: (75)
|
Hello SIOS-Forum-Conmmunity
If possible, boundary conditions (e.g. data sheet) of the printer to be connected should be avilable in advance. This can provide information such as:
The OUC (Open User Communication) is used for communication between the SIMATIC controllers via Industrial Ethernet. In addition to the manual of the SIMATIC controllers, some entries are available in the SIOS portal: Libraries for Communication for SIMATIC Controllers SIMOTION, SIMATIC: Communication Library LCom for Ethernet Communication Basic Examples for Open User Communicacion (OUC) How do the instructions TSEND_C and TRCV_C behave in the S7-1500? With Best Regards, SIMATIC International Technical Support Hub |
Follow us on