12/7/2020 11:07 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1051)
|
hi ductoan2503, I would try to reset the interfaces. See this FAQ: How do you generally parameterize the PG/PC interface and how do you ensure that the device driver can be selected and is visible?Also check if the Windows services are started. Have a look in the Windows-services and check if the SIMATIC S7DOS-help-service is working. hope this helps, regards, |
FCK WAR! |
|
This contribution was helpful to2 thankful Users |
12/12/2020 6:36 AM | |
Joined: 1/1/2017 Last visit: 6/6/2024 Posts: 330 Rating: (11) |
Thanks a Lot! |
Follow us on