4/22/2015 11:32 AM | |
Posts: 94 Rating: (0) |
Hi Daniel , Now Two thing i need your help : 1. After successful connection , i am able to recieve data from S7200(226) .I am using 16 byte i/o buffer in s7300 configuration as i have to collect 3 floating point and 2 integer value from S7200 . But i am recieving some garbage value/ different value . Kindly suggest me some better solution on this . 2. I have to connect another S7200(222 CN) with another Master via em 277 Profibus module . Baud rate set for profibus -9.6 kbps Terminating resistor is on in both side (Master and Slave). Profibus cable is connected in incoming(A1,B1) in both side . But i am not able to detect the node from master side . EM 277 module CPU-falut is blinking in every 5 sec . Kindly suggest me the possible reason for CPu Fault and solution. Thanks in advance .
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 4/22/2015 12:02:45 PMNew subject after splitting |
|
Follow us on