1/13/2017 2:01 PM | |
Posts: 7 Rating: (0) |
I used S7-Lan converter (http://inee.pl/produkty/s7-lan). I can connect to S7-300, upload software, and hardware (Step7). I can go online (in Step7 online mode i see all profibus nodes - in hardware configurator) but then i try option "display accessible nodes" (on Step7 or Starter) I can't see the inverter profibus address. Did I must set or check someting else in starter or in inverter? The ProfiBus speed is set to 1,5Mb/s. |
Last edited by: kulawikm at: 1/13/2017 2:02:29 PM |
|
1/13/2017 3:05 PM | |
Joined: 5/12/2006 Last visit: 4/23/2024 Posts: 22224 Rating: (2979)
|
can you make a screen of accessible nodes? the DP Adress on the G120 is set correctly with the dipswitches? |
Follow us on