8/31/2021 12:10 PM | |
Joined: 10/10/2005 Last visit: 4/18/2024 Posts: 1917 Rating: (133) |
Hello dusszeq, there are some applications (example programs and descriptions) in the internet. Perhaps it could be helpful for you: Greenhouse control with SIMATIC S7-1200 Creating and using user-defined web pages on S7-1200 / S7-1500 Getting Started SIMATIC S7-1500 Cicero |
8/31/2021 1:35 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1051)
|
hi, S7-1200 provides also an OPC UA Server. You just need to activate it and install a OPC UA client on the PC-station.For more information about it, have a look into this FAQ and application samples: OPC UA-Server of the S7-1200 CPUsModeling the S7-1200 OPC UA Server interface in TIA Portalhope thie helps, regards, |
FCK WAR! |
|
Follow us on